9/6/2024 3:09 PM | |
Joined: 2/1/2010 Last visit: 10/3/2024 Posts: 150 Rating: (71) |
If you are inquiring about ExtVal### inputs, those are basically used for customization of the message text using text substitution. You can find this info in the manuals/PUD. From PUD: "The associated values4 ... 8 are allocated to the parameters ExtVa104 ...ExtVa108 and can be used. Additional information is available in the "Process Control System PCS 7 - Engineering System" manual." iirc associated values line up with MsgEvId1 = 104-108 and MsgEvId2 = 204-208, etc. if there are many MsgEvId# in a block.... |
If my post helped you, please rate. Thanks. |
|
Follow us on