12/20/2016 1:26 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
This Application Example shows how to use the SIMATIC IOT2000 to communicate with an S7-1500 PLC via S7 communication
AttachmentS7_Comunication_node-red_V1.0.pdf (18548 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to3 thankful Users |
12/21/2016 2:01 AM | |
Joined: 5/4/2011 Last visit: 4/19/2023 Posts: 16 Rating: (2) |
Dear bergmanu, this is so helpful that we can realize many many applications..... |
1/9/2017 2:43 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi davide_maffei, with Date_And_Time it is not that easy, because it uses the BCD format. If possible use DTL instead, it is more easy. Is it possible for you? Here is some documentation but not really a list: https://github.com/plcpeople/nodeS7/blob/master/README.md I am testing it with Date_And_Time at the moment. Since now I only had success with DTL. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/9/2017 3:01 PM | |
Joined: 3/17/2014 Last visit: 1/15/2024 Posts: 53 Rating: (12) |
Thank you bergmanu! I tried also with DTL but I cannot read the whole variable using the same address posted in my first topic. In this case I have to read the variable as an Array splitted in the USInt element Year,Month,....etc ? Best Regards
|
2/27/2017 4:10 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi JDarius,
I attached an example which uses the IOT2000 time as timestamp. If you synchronize your PLC and your IOT with the same ntp server, this should be a good way.
Yes this would trigger every second, if the timestamp format changes every second.
S7 connection is no problem with PLCSim Advanced. So this should work, but I have to check this too.
Do you have connection to your PLCSim Advanced? Ping is possible? If not make sure that you selected "Virtual Ethernet Adapter" in your PLCSim settings. Are there some errors displayed by node-red? AttachmentData+Timestamp.txt (1544 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
3/13/2017 5:09 PM | |
Posts: 7 Rating: (0) |
Hi Hugo, have you tried using "db1,X0.0" instead of "db1,bool0" ? Best Regards, Tiago Machado |
3/28/2017 8:45 AM | |
Posts: 71 Rating: (16) |
To install packages using npm you need an internet connection. |
This contribution was helpful to1 thankful Users |
3/28/2017 9:10 AM | |
Posts: 71 Rating: (16) |
Yes, sorry, I mixed up left and right there. JDarius' comment is correct. |
3/31/2017 7:31 PM | |
Posts: 7 Rating: (0) |
I have some good news ! Now the S7 node also supports the write function. |
This contribution was helpful to3 thankful Users |
4/3/2017 8:32 AM | |
Posts: 215 Rating: (6) |
Do I need to give this command in a specific directory, or can I run this in root? |
7/14/2017 10:58 AM | |
Joined: 5/22/2014 Last visit: 4/17/2018 Posts: 32 Rating: (1) |
Hi guys, I would like to know if it is posible to program the same but using C++ ;) Thanks you! |
7/14/2017 12:59 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, I think you already found it ;) https://support.industry.siemens.com/tf/ww/en/posts/snap7-iot-for-quark-iot2000-platform/158392/?page=0&pageSize=10 Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
5/22/2018 10:57 AM | |
Posts: 1 Rating: (0) |
Hello, |
5/2/2019 11:37 AM | |
Posts: 8 Rating: (0) |
Hi all, I'm trying to get a boolean value of a level sensor out of a S7-1200 PLC using this guide. Could anybody please confirm if I'm doing this correctly? I can't seem to get the IOT2040 to create the file with the variables. [snip] Thanks in advance, Connor AttachmentScreenshots.zip (1000 Downloads) |
Last edited by: Cannuh at: 05/02/2019 11:38:36Last edited by: Jen_Moderator at: 05/03/2019 10:25:25Removed link and added file as an attachment. |
|
5/8/2020 12:44 PM | |
Posts: 12 Rating: (0) |
Hello, I set up everything like describe in the documentation. But I always receive the error “wrong value”. Does anybody see the error in my settings? Best regard! AttachmentPictures.zip (926 Downloads) |
7/28/2020 10:37 AM | |
Joined: 6/19/2017 Last visit: 6/3/2024 Posts: 8123 Rating: (165) |
Hi Edinson Caceres, we decided to use englisch as language for posts, because this is an international forum, where users from all over the world helping each other. So please use englisch for your posts. ___ Translation:
Best regards, |
My Forum is the place to personalize your profile, |
|
2/17/2021 2:32 PM | |
Joined: 1/9/2018 Last visit: 4/30/2024 Posts: 2 Rating: (0) |
Thank you very much, problem solved ;-) |
This contribution was helpful to1 thankful Users |
Follow us on