(0)| 1/4/2026 7:13 PM | |
|
Joined: 9/21/2012 Last visit: 1/15/2026 Posts: 4848 Rating:
|
What do you have on th USB drive? Is it the 2nd generation basic panel recovery files from SiePortal? |
| 1/14/2026 10:50 AM | |
|
Joined: 8/14/2020 Last visit: 1/14/2026 Posts: 450 Rating:
|
Hello juan_gomez161 I'm not entirely clear on what you're trying to achieve with the USB stick and the KTP700. Could you describe your goal in more detail? Otherwise, if you want to perform a factory reset on the KTP700, please see the following link: It's possible that certain USB sticks won't be recognized. For the specific application "USB Recovery Stick," the following limitations apply: -> USB version <3.0 -> FAT32 formatting The following USB stick 6AV2181-8AS20-0AX0 should work Best regards, Costanza |
| 1/14/2026 2:11 PM | |
|
Joined: 8/14/2020 Last visit: 1/14/2026 Posts: 450 Rating:
|
Hello juan_gomez161 I hope the USB sticks you tried are no larger than 8GB? If they are larger than 8GB, that could be the reason. Otherwise, if you used the Siemens USB stick 6AV2181-8AS20-0AX0 https://support.industry.siemens.com/cs/us/en/pv/6AV2181-8AS20-0AX0/pi?dl=en and the panel doesn't recognize it, I am not aware a other way to get the panel working again. The only remaining option is to send it in for repair. |
| 1/15/2026 12:44 PM | |
|
Joined: 7/31/2020 Last visit: 1/15/2026 Posts: 483 Rating:
|
Hello, Were the USB sticks also formatted to FAT32, as Costanza specified? Best regards |
Follow us on