10/27/2022 3:42 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263) |
The last BIOS Update (V14.01.07) is for the SP 305.
You can download it from here: BIOS downloads for SIMATIC IPCs, SIMATIC Tablet PCs, SIMATIC Field PGs, SINUMERIK PCU and SIMOTION P320 |
10/27/2022 1:21 PM | |
Joined: 12/24/2014 Last visit: 7/12/2024 Posts: 14 Rating: (0) |
I can't download the file, I don't have permission. Despite periodic attempts to complete registration. |
10/27/2022 1:28 PM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263) |
Yes, you need a extended registration. The download is export restricted. |
10/27/2022 1:33 PM | |
Joined: 3/11/2019 Last visit: 11/8/2024 Posts: 1653 Rating: (305) |
Hi, unfortunately, download is not possible without a registration for export restricted products. You can check following FAQ , if not already done. But you have to wait till your account was checked. Why do you have to log in and register for downloading export-restricted software and what data do you need for this?regards sancruz |
Feedback appreciated, please rate |
|
10/28/2022 1:58 AM | |
Joined: 12/24/2014 Last visit: 7/12/2024 Posts: 14 Rating: (0) |
Yes, I know. I try to do this several times a year, I fill out the form, send it, but there is no result ... |
10/28/2022 3:46 AM | |
Joined: 12/24/2014 Last visit: 7/12/2024 Posts: 14 Rating: (0) |
Ok. I found the latest firmware, updated the bios, but still the SP306 battery is not charging... |
10/28/2022 3:54 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263) |
Start a Support Request ... |
Follow us on