3/1/2012 1:28 PM | |
Posts: 739 Rating:
|
Hi, If every thing is well outside of inverter, it might be a defect inside. notes to motID: - if output chokes, output filters, contactors, long cables (and so on) in use,. MotID will not work properly and should done manually. FAQ: http://support.automation.siemens.com/WW/view/en/37690358 - with multimotor, MotID will not work - with synchronus, motor MotID will not work |
5/9/2014 9:08 AM | |
Joined: 3/2/2007 Last visit: 9/9/2025 Posts: 990 Rating:
|
how did you solve this problem? |
... thank you ... |
|
5/9/2014 9:21 AM | |
Posts: 46 Rating:
|
Please advise how this issue was solved |
5/10/2014 4:09 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
If you are facing same proble, kindly mention details about the fault When it occurs? During starting or during running? Any alarm occurs during this ? have you checked resistance of Motor including cables from terminal itself?? (Do not disconnect cable) Also have a look at following discussion https://www.automation.siemens.com/tf/WW/en/Posts/28101 Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on