5/14/2018 9:59 AM | |
Joined: 4/3/2018 Last visit: 11/7/2019 Posts: 3 Rating: (0) |
Hello, I have similar problem with vbscript after updating to SP1 and updates(1-5) didn't help me. I have script which was working for a years on previous versions of wincc 7.x, also with wincc 7.4. I had also problem with basic IF conditions, but i solved it with replacing each conditions. For example: If (a=0) And (b=1) Then do sth. End If Script like this didn't work, but after replacing the condition like this: If (b=1) And (a=0) Then it started working. Did anyone have a similar problem? Or any ideas? Thanks a lot. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/14/2018 2:21:43 PMNew subject after splitting |
|