3/30/2024 6:17 PM | |
Joined: 2/4/2024 Last visit: 4/23/2024 Posts: 7 Rating: (0) |
Simodrive 611 A. Good afternoon everyone here. I'm asking for help again following a problem I've already posted before, about errors F09 and F19, on the controller board 6SN1121-0BA11-0AA0 E-stand version A. I looked for used boards and found several, all around 700 euros and more, but with no guarantee that they were working, so I decided to repair the main board and secondary boards, changing all the electrolytic capacitors that had low capacity and ESR high. I will also change the LM12458CIV chips on board 46200.9232.04 and 462008.7261.03, and test boards after changing the ICs. Another question I have is about the slot where the 462008.9232.04 subboard fits, I think it is this subboard that controls the incremental encoder, ERN1387. When I received the controller board to repair this subboard 46200.9232.04, it was fitted in slot X13 on the main board, but from what I analyzed after measuring continuities between Plug X12, where the encoder plug connects, and the board sockets 6SN1121-0BA11- 0AA0, I think this subcard should be fitted in slot X14. Am I correct? can anyone confirm? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Fertec.Fertec at: 03/30/2024 18:19:15Last edited by: Fertec.Fertec at: 03/30/2024 18:34:28Last edited by: Fertec.Fertec at: 03/30/2024 18:34:46Last edited by: Fertec.Fertec at: 03/30/2024 21:47:10Last edited by: Fertec.Fertec at: 03/31/2024 15:44:10Last edited by: Jen_Moderator at: 04/02/2024 07:45:37New subject after splitting |
|
4/2/2024 7:46 AM | |
Joined: 6/19/2017 Last visit: 5/23/2024 Posts: 8095 Rating: (165) |
Closed cause question posted twice. The second thread with the subject Simodrive 611 A_6SN1121-0BA11-0AA0 E-stand version A is published within the conference SIMODRIVE Converter system. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on