8/11/2010 6:50 PM | |
Posts: 11 Rating: (0) |
Well, I attach a PDF servovalve manual in this response, if you see i have the servovalve without the electronic part so... i need 2.7W at least. AttachmentServovalvula parker.pdf (511 Downloads) |
8/19/2010 12:46 PM | |
Joined: 9/23/2005 Last visit: 6/11/2024 Posts: 4346 Rating: (1433)
|
Hi, excuse again. In this context, really your S7-1200 could not drive too high current (it is limited to something like 10mA). Siemens has a interface converter: 3RS1700-2AD08-0AC0 INTERFACE CONVERTER 0-10V/0-10V UC24V http://support.automation.siemens.com/BR/view/en/26365212/tdhowever I don't think that it could drive so high current too. Maybe is wold be better to use a servovalve with eletronic. |
Denilson Pegaia |
|
Follow us on