2/18/2022 10:22 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating:
|
Hi, Do you want to download the firmware? (this is necessary to upgrade the firmware of CPU) But you are telling, that online already has FW4.2.1 In TIA Portal v14, you select the firmware v4.2 Best regards, Wizard |
2/18/2022 11:07 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating:
|
Hi, Have you seen this thread: Best regards, Wizard |
2/18/2022 1:05 PM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
|
Last edited by: Ahoora - Jafari at: 02/18/2022 13:10:36 |
|
2/18/2022 2:42 PM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating:
|
Hello, I guess you have not installed WinCC Comfort v14. (Because you have not TP1500 Comfort panel) (See Help -> installed software) What version of TIA Portal v13 have you installed? Including Service packs and updates? Best regards, Wizard |
2/18/2022 3:21 PM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
|
Last edited by: Ahoora - Jafari at: 02/21/2022 09:58:10 |
|
2/18/2022 3:39 PM | |
Joined: 7/7/2010 Last visit: 6/14/2024 Posts: 14802 Rating:
|
If you use TIA Portal V15 or higher and use "online access" from the project tree, you can expand the "General" tab to see the version of TIA Portal used to compile the project loaded in the PLC. V13 definitely does not show the Portal version required to upload from the PLC. V16+ definitely shows it. It's worth installing V16 or V17 just to see the portal project version details via the online access method. |
science guy |
|
This contribution was helpful to
2 thankful Users |
2/22/2022 3:57 PM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
Thanks mate That make more sense now By the way, I think something is wrong with my TIA 14 as well because it doesn't show any hardware for TP1500 comfort!!! I decided to uninstall version 14 (SP1 + Update 3) and install it again + install version 16 as well (I tried Version 17 but I couldn't even see online Hardware's (PLC/HMI) the same as TIA 13). By the way, even Prosave V13 or V14 says: hardware's are not the same (TP1500 comfort) and won't let me to make a Backup of HMI... I've used prosave on different TP1200 comfort panels and upload it in a few seconds but not this panel! Thank you very much for the help |
2/22/2022 10:36 PM | |
Joined: 7/7/2010 Last visit: 6/14/2024 Posts: 14802 Rating:
|
If a panel was not loaded with a configuration setting that allows for the HMI to be "uploaded", you cannot perform an upload of the HMI. Perhaps that is the problem with that one HMI. |
science guy |
|
This contribution was helpful to
1 thankful Users |
2/23/2022 8:30 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating:
|
Hello, Did you install WinCC Comfort v14? (If not, you can not select Comfort panel in your project) In Prosave did you select TP1500 Comfort or TP1500 Comfort v2? Best regards, Wizard |
2/23/2022 8:58 AM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
Morning, I am trying to install it today. TP1500 Comfort was selected not anything else. |
2/23/2022 9:09 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating:
|
Hi, What is the MLFB number of the panel? 6AV...… Best regards, Wizard |
2/23/2022 9:41 AM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
6AV2 124-0QC02-0AX0 C-JON74757 28-63-36-E7-6C-17 Mac Address when I try to read the HMI status by Prosave (TIA13 or 14 or 17), it doesn't show any MLFB or ... and just says, |
Last edited by: Ahoora - Jafari at: 02/23/2022 09:43:31Last edited by: Ahoora - Jafari at: 02/23/2022 09:46:28 |
|
2/23/2022 10:23 AM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
You were right, I managed to find the version by using TIA 16 or 17 (My TIA 17 was on a notebook and I had some problem with Ethernet setting for USB to RJ45). [snip] |
Last edited by: Ahoora - Jafari at: 02/23/2022 11:27:35Last edited by: Ahoora - Jafari at: 02/23/2022 11:28:32Last edited by: Jen_Moderator at: 02/24/2022 07:21:03Division of questions into separate topics. |
|
2/24/2022 7:20 AM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating:
|
New question published by Ahoora - Jafari is split to a separate thread with the subject How to install update on TIA 13?. Best regards |
My Forum is the place to personalize your profile, |
|
2/24/2022 9:34 AM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating:
|
Morning again, These are new print screen of what I have found. Hope somebody find a way to upload the project otherwise I HAVE TO WRITE THE CODES AND SCREEN FROM SCRATCH OR BY OPENING ANY FUNCTION AND COPY PASTE THEN MODIFIY THEM TO SUIT NEW HARDWARE. THANKS |
Follow us on