9/11/2024 1:41 PM | |
Joined: 3/30/2020 Last visit: 10/13/2024 Posts: 4858 Rating: (992) |
Some functionality has been added to the S7-1500 FW:V2.9 that may be of help. See DHCP in the following article: New firmware version V2.9.. Consider contacting Siemens if you cannot find anymore information. - It is possible to change the IP address of the PLC (S7-1200 / S7-1500) in runtime. Though I am not sure if the S7-1200 needs to go through a power outage to apply the address. In theory you could make a user program that changes the IP if you have a way of triggering the task and can detect the missing IP. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on