(0)| 2/16/2025 1:31 PM | |
|
Joined: 12/12/2023 Last visit: 2/16/2025 Posts: 1 Rating:
|
Hello! I have ABB Softstarter PSTB370-600-70 When the 220V panel power is connected, there is access to the menus and there is no problem. However, when three-phase input power is supplied, it gives a message Uin Not Ok when a motor load is connected to the output. When the load is lifted message Uin Not Ok disappear. What could be the possible reason? Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/17/2025 10:23:18New subject after splitting |
|
Follow us on