10/28/2021 10:08 AM | |
Joined: 1/11/2019 Last visit: 9/3/2024 Posts: 755 Rating:
|
Hello Masood_Es, It is bit difficult to give you the project program solution over here. You have to use either MotL or MotS block with Channel drivers in CFC to control the field motor pumps. Those mentioned blocks are available in APLibrary. You can go through the below link to know about CFC (Getting Started) & You can surf below link to know about APLibrary blocks PCS 7 Advanced Process Library (V9.0 & Use below link for PCS7 getting started PCS 7 Getting Started - Part 2 (V9.0 with APL) Hope it helps you! |
10/28/2021 12:19 PM | |
Joined: 3/13/2015 Last visit: 8/27/2024 Posts: 136 Rating:
|
Dear Masood_ES, It sounds like you should take a look at the Aggr08/16 function provided with Industry Library:
With this block you can start multiple pumps, order based on operating hours. With best regards, |
Last edited by: Molthoff at: 10/28/2021 12:21:33 |
|
This contribution was helpful to
1 thankful Users |
10/29/2021 8:49 PM | |
Joined: 9/8/2015 Last visit: 8/27/2024 Posts: 116 Rating:
|
Thank you very much! Your answer is exactly what I wanted. |
10/30/2021 7:58 AM | |
Joined: 9/8/2015 Last visit: 8/27/2024 Posts: 116 Rating:
|
I check this function, but where is not in pcs7 v9!!! |
Follow us on