1/10/2023 4:16 PM | |
Joined: 1/6/2023 Last visit: 1/30/2023 Posts: 3 Rating: (0) |
Hi, to be start with, I am having a two pump system hookep up with S7 200 Microwin. There were 2 unit of sinamics G110 drive attached to PLC with USS RS485 communication. I replaced one of the drive to Sinamics V20 model today and set bus address and other parameter follow my old Sinamics G110. However, my system does not start and there is no any error msg on sinamics V20. Do I miss anything while do the conversion? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/11/2023 09:21:32New subject after splitting Last edited by: Jen_Moderator at: 01/11/2023 09:24:46Spelling mistake removed from headline. |
|
1/11/2023 3:24 PM | |
Joined: 10/11/2006 Last visit: 10/9/2024 Posts: 5910 Rating: (808) |
Hello, |
With best regards, |
|
This contribution was helpful to1 thankful Users |
1/25/2023 1:00 PM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (1) |
Hi Use USB-PPI PLC Programming CABE USB to RS485 Adapter and check out this video.
|
Last edited by: Jen_Moderator at: 01/25/2023 13:06:57Video embedded. If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
Follow us on