6/10/2023 1:31 PM | |
Joined: 6/10/2023 Last visit: 6/21/2023 Posts: 3 Rating:
|
Can anyone help me with this project(chemical dosing pump) using logo siemens software: When you press the start push button, it should actuate a solenoid valve and a flowmeter and discharge 98litres of water into tank A, and also actuate another solenoid valve and a flow meter and discharge 2 litres of chemical into tank A. when the low level sensor in the tank A is activated, the counter should reset back to zero and start the process all over again. The components: A start push button, stop push button, high level sensor and low level sensor in tank A, a flow meter and solenoid valve for water, a flowmeter, solenoid valve and pump for chemical, a low level sensor in the chemical tank. AttachmentAutomation project.pdf (541 Downloads) |
Last edited by: kolawole_oyewo192 at: 06/10/2023 17:12:28Last edited by: kolawole_oyewo192 at: 06/10/2023 18:55:55 |
|
6/10/2023 2:14 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
Too little information. |
6/11/2023 5:38 PM | |
Joined: 6/11/2019 Last visit: 9/6/2024 Posts: 2247 Rating:
|
With a 2nd counter. But please upload your program so that we can understand it. |
6/12/2023 7:16 AM | |
Joined: 6/10/2023 Last visit: 6/21/2023 Posts: 3 Rating:
|
What information do you need |
Follow us on