6/29/2024 8:24 PM | |
Joined: 6/22/2024 Last visit: 9/14/2024 Posts: 2 Rating: (0) |
Kindly I'm using a logo PLC to create a three booster pump. Pump dry run protection is the first input; duty selection presser switch is the second; and assist pump run pressure switch is the third. Pump 1 failure is the fourth input; pump 2 failure is the fifth; and pump 3 failure is the sixth. I came up with a reasoning that says the remaining working pumps must continue to function continuously if one or more pump is fail. Please send this operation rationale; I've been trying for a long time. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 07/01/2024 13:06:24New subject after splitting |
|
6/30/2024 3:50 AM | |
Joined: 12/18/2014 Last visit: 10/10/2024 Posts: 33927 Rating: (4217)
|
What is your idea? Or do you expect a complete program? |
7/2/2024 3:50 AM | |
Joined: 6/22/2024 Last visit: 9/14/2024 Posts: 2 Rating: (0) |
I programmed for my application but when two pumps trip, the healthy pump is not working. Please check and advise if anything is wrong If possible, send a compliant programming for us
AttachmentKhalifa 3 booster pump.zip (290 Downloads) |
Follow us on