10/7/2024 5:40 PM | |
Joined: 6/4/2008 Last visit: 10/8/2024 Posts: 1501 Rating: (324) |
Hi, as long as the motors have individual protections, then I would leave it as a single drive i.e. a G130 drive unit (200 - 250kW based on the duty/loading cycles etc) or G150 if you wanted to replace the entire cabinet. Take a look at the CATALOG Using S120 with individual modules, even double motor modules would be horrendously expensive. Regards, Graeme |
Follow us on