9/17/2015 7:58 AM | |
Joined: 2/20/2014 Last visit: 8/18/2024 Posts: 396 Rating:
|
Hi there, I need help to complete this program. The program need to have at least one pump running when the first two level is true. and the other pumps need to run when more levels is true. Currently i have done writing the program where pump will take turn to run where first time the level is true, first pump will run and the next round it will run the next pump and it continues. I am having problem now to get more pump running when more levels is true, Please help. Thank you in advance, Attachmentnormal_1P_RS_2015SEP17.zip (289 Downloads) |
9/17/2015 9:16 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating:
|
You have make a hugh programm. Next time you make a programm make it in FBD. Its mor flexible, better to edit, better to understanding etc.
If pump 1 running 10 minits (example) its not enough, then pump 2 must als strating? So you can make more, after an other 10 minuts you can start pump3 and so on. Attachmentpumps.zip (285 Downloads) |
This contribution was helpful to
1 thankful Users |
9/21/2015 2:41 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
Hello karthirkk, pity that they do not respond. That is why I once made something out ready on pure conjecture. Attachmentkarthikk.zip (258 Downloads) |
This contribution was helpful to
1 thankful Users |
9/25/2015 11:08 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
Hello karthikk, I once dealt me a little closer to your task and created this program. Attachmentpump_sequence_V2.zip (363 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on