Industry Online Support
Technical Forum
9/5/2007 11:13 AM | |
Joined: 10/31/2006 Last visit: 9/21/2022 Posts: 134 Rating:
|
Here is a small example to get you going. Create 4 Internal tags T12345_DESCRIPTION ( DataType - Text ) T54321_DESCRIPTION T12345_VALUE ( Data Type - Floating Point ) T54321_VALUE Put some start values in these tags so you can see the values when you open the template We mostly use Structure Tags for these type of applications ( pumps , valves etc ) as it makes the engineering a lot easier and everything is uniform. Check the properties of the picture window to make it behave ( movable, in the foreground , borders etc ) how you want. Regards Shane AttachmentPicWindow.zip (231 Downloads) |
Last edited by: CromptonS at: 05.09.2007 11:17Last edited by: CromptonS at: 05.09.2007 11:15 |
|
This contribution was helpful to
1 thankful Users |
3/24/2008 2:07 PM | |
Joined: 5/17/2006 Last visit: 2/26/2024 Posts: 218 Rating:
|
Thank you so much , Its very simple and understandable example Best regards |
Genetic Fuzzy PID Controller |
|
Follow us on