8/12/2018 5:53 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
V20 drive works on 0-20 mA , AI2 & 0V. Please refer SINAMICS V20 Inverter for more detail information. |
Last edited by: Jen_Moderator at: 8/13/2018 10:51:36 AMOptimized link. |
|
8/13/2018 5:21 PM | |
Joined: 3/27/2008 Last visit: 11/12/2024 Posts: 1147 Rating: (142) |
The attached may help with this application. Use Cn0008 or Cn0009. The default settings should provide a place to start with the settings, or see the attached. I have done this with cooling water pumps in a Jam factory to regulate the cooling water to pressure. Also the cooling tower regulation was successful using temperature in the water, and controlling by using speed control for the fan. AttachmentV20 PI control.docx (493 Downloads) |
Last edited by: tractor at: 8/13/2018 5:26:01 PMTractor |
|
Follow us on