7/10/2018 4:40 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hello together, attached you can find an example how to use a 3G mPCIe card for having conenction to the internet. I hope you can make use of this since many people are asking about 3G connection Best regards! AttachmentIOT2000_Modem_via_mPCIe.zip (2358 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to7 thankful Users |
12/18/2018 11:47 AM | |
Posts: 1 Rating: (0) |
Someone have tested other models? i.e. Huawei MU709s-2phttps://www.amazon.es/Huawei-MU709s-2-minicard-MU709s-2p/dp/B01DB3YKH6 |
1/30/2020 12:33 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, You can transfer files using WinSCP -> SFTP -> port 22 |
This contribution was helpful to1 thankful Users |
6/23/2020 4:07 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, we used this one. This is a german link, but I think you can see the model used. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
7/26/2020 11:28 PM | |
Posts: 9 Rating: (0) |
Dear all, I'm trying to configure a TELIT LE910C1-EU modem in IoT2040 and followed the steps indicated in the exampled posted by bergmanu, but it seems that the new interface is not recognized and I canot connect to Internet. I attach the following pdf file with all the steps that I've done: "Problems configuring modem TELIT LE910C1-EU with IoT2040.pdf". Please, any help, comment or hint on how to go on will be very wellcome! Thank you!. AttachmentProblems configuring modem TELIT LE910C1-EU with IoT2040.pdf (823 Downloads) |
7/27/2020 3:56 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Please try flashing a fresh image and configuring the card over cellular options in:
Kind regards! |
7/29/2020 11:50 AM | |
Posts: 22 Rating: (0) |
I´ve got the same problem! but also with the huawei Mu609 Did you solve it? |
7/31/2020 1:01 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, We figured the Application example PDF is only working correctly with Image V2.2.0. If you want to use this method, you can send me a PM with an Email Address and I can provide you this Image. Configuration over iot2000setup requires some additional steps:
Kind Regards!
|
8/1/2020 5:50 PM | |
Posts: 9 Rating: (0) |
Hello Fe_lipe, I think I did correctly all what you mentioned (still with image V2.6.1), but without success! Please see the attached word file with the steps. I'm waiting for you to send me the image V2.2.0. Thanks! AttachmentIoT2040 modem configuration.docx (774 Downloads) |
8/3/2020 1:28 PM | |
Posts: 24 Rating: (0) |
Hi Bergmanu, I have tried your last steps in the post, but I am still not able to connect. In fact, I have used the v2.2.0 but when I enter on iot2000setup / networking, I only see eth0 and eth1, no celular is defined. In the same line, when I type ifconfig, I only have lo, eth0 and eth1. Nevertheless, I have in my /etc/network/interfaces file the modem one configured. Please see attached the screenshots and the log file. It seems that the ttyUSB0 is lock by another pid… and that is why it is not able to connect. Best regards, Laura Attachmentmodem configuration IOT2040.zip (746 Downloads) |
8/4/2020 8:05 AM | |
Posts: 22 Rating: (0) |
something is wrong... making all things that should work fine with mu609 but still unsuccefull results... |
8/5/2020 10:38 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello zbazan, I just sent you the Image V2.2.0, please try once again using the PDF description and script files. I hope it works out. @laura: We noticed the configuration for your card is not working correctly over iot2000setup even though the drivers seem supported by the kernel. We will investiagte further and see if we can configure your card manually with AT commands over the serial interface. Meanwhile please open an issue on here. And describe the exact behavior with "ofono not running" and the Model of your Telit card. Kind regards! |
8/5/2020 11:38 AM | |
Posts: 22 Rating: (0) |
Not working.... cellular not appears in iot2000setup.... not pap or chap file an my provider file is not the same as you posted @fe_lipe |
8/7/2020 11:19 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Thats unfortunate. What does
output? |
Follow us on