5/23/2017 8:29 AM | |
Posts: 32 Rating: (0)
|
Please feel free to post your questions, tips and proposals regarding "SINAMICS Rotary Knife/Cross Cutter" topics here. For all other applications or general topics please refer to the corresponding thread. |
4/17/2018 7:51 AM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello, if you want to use a S120 drive system, I would recommend to use the application example "S120 Crosscutter with DCB Extension". https://support.industry.siemens.com/cs/ww/en/view/109477746 For this kind of crosscutter, you need a S120 drive and a runtime license called DCB Extension. There is also a SIMATIC block for the application, that can be used with a S71200/1500 PLC. This block is used as a control of the drive and also to control the crosscutter functionalities. With the ready to use block you can for example switch on the drive, enable the cutting operation and start the cutting process. You can create then an HMI on your own to trigger the inputs of this ready to use function block. You can find more information in the manual of the crosscutter, there are also some basic information of crosscutters available. The manual can be found in the link that I attached above. If you are interested in the application, then I recommend to contact you local siemens contact, which can be found here: https://www.automation.siemens.com/aspa_app/?cntryid=DE&lang=en Another tip: Besides the S120 crosscutter application example, there is also a solution with SIMOTION: https://support.industry.siemens.com/cs/ww/en/view/37706606 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
5/11/2018 2:10 PM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello, I suggest to contact your local siemens contact, which can be found here: https://www.automation.siemens.com/aspa_app/?cntryid=DE&lang=en Just say that you want to have the demoproject for SIMOTION rotary knife and they will provide it. |
With best regards, |
|
8/3/2018 11:44 AM | |
Posts: 3 Rating: (0) |
Hi, I want to download technology package 'TPGMC_SINAMICS_4_8.4.1 V4.80.4.1' . Pls send the link. -Pradeep |
8/3/2018 1:48 PM | |
Posts: 3 Rating: (0) |
Dear Sir, Thanks for the support. -Pradeep |