3/1/2024 1:35 AM | |
Joined: 4/28/2015 Last visit: 8/16/2024 Posts: 17 Rating: (3) |
Very good FredrikS7. It worked fine here. I have now LSC v8.4 running on my macOS 14 (Sonoma). You made my day. I tried the same trick on my macOS 11, and it worked too. By the way, this is the same macOS on which I was working on with Siemens support to get the upgrade installed. I will tell them the good news. For those that have not followed from the beginning, I have made an instruction sheet that explains the steps to do to be able to install the upgrade to LSC v8.4 on macOS 14. It works also on mac OS 13, but with a little difference (see PDF). AttachmentInstall Upgrade LSC v8.4.pdf (522 Downloads) |
Last edited by: Bruno_994324 at: 03/01/2024 02:16:37Last edited by: Bruno_994324 at: 03/01/2024 02:17:05Last edited by: Bruno_994324 at: 03/01/2024 16:33:43 |
|
This contribution was helpful to2 thankful Users |
Follow us on