Industry Online Support
Technical Forum
6/5/2012 10:24 PM | |
Posts: 19 Rating: (0) |
Firmware 1.0, is that the problem ? do i need to update the firmware ? |
6/6/2012 6:33 PM | |
Posts: 19 Rating: (0) |
thanks for your advice! now, i would like to know where can i buy the update Memory Card ? best regards...
|
6/7/2012 5:52 AM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello SSJV, Now buying a Memory Card only for the purpose of upgrading the firmware may not help. Hold on for some time till we get some official information. As currently the S7-1200 System Manual (04/2012)says "Note You cannot update an S7-1200 CPU V2.2 or earlier to S7-1200 V3.0 by firmware update." So try to do the firmware update with the help from your local siemens representative. |
Like it? Rate it! |
|
Follow us on