12/1/2022 12:04 PM | |
Joined: 7/19/2022 Last visit: 11/11/2024 Posts: 419 Rating: (71) |
Hi AutoGen_6815244, I'm afraid that if you are using WinCC Advanced and you want to show in a graph for example the last 100 values of a variable it will not be possible. Keep in mind that WinCC Advanced is still the HMI like a panel but on a PC, so it has more limitations than WinCC for SCADA (WinCC Professional) where you can dynamize absolutely everything in the curve viewer and therefore you could implement what you are looking for. What it does allow you to do is to show the history of all the variables stored in the curve viewer, but not individually and by a specific number. |
Last edited by: JBS98 at: 12/01/2022 12:07:02If this Information really helps, you could use the Rate function |
|
Follow us on