4/10/2024 10:19 AM | |
Joined: 7/19/2022 Last visit: 4/30/2024 Posts: 356 Rating: (60) |
Hello Tejus, In WinCC Advanced, the dynamization of objects such as lines is somewhat more limited. You can animate the color of the line but depending on the value of a tag and not on the comparison of two tags. Another option would be to create a script that compares the values of two tags and depending on the result change the color of the line. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on