7/7/2023 10:46 PM | |
Joined: 5/20/2017 Last visit: 4/9/2024 Posts: 3 Rating: (0) |
Good day I have step 7 5.6 and I could see projects with solution line components, when I upgrade to Step 7 5.7, I can't see the same project with solution line components, I need the correct toolbox with SL libraries but to version of step 5.7 but i could not find. Please Can you help me? Tanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/10/2023 10:44:49New subject after splitting |
|
7/10/2023 10:02 PM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating: (353) |
Don't know what is meaning "can't see the same project with solution line components" How many PG/PC with STEP7 you have, use the one which you can see or downgrade to the old STEP 7 version If you don't find 840D Toolbox in the Lib, search the whole PG/PC HDD nomallay showing like "gp8x0d Va.b" V==Version, a=1..6,7 b=3...5,6,7.. if you don't find any in your PC, you need contact local Siemens office to order SINUMERIK 840D sl Toolbox Version 5.7
|
If you like my comments please |
|
6/14/2024 10:59 AM | |
Joined: 6/14/2024 Last visit: 6/28/2024 Posts: 1 Rating: (0) |
I have the same problem, did you solve it? |
6/14/2024 1:05 PM | |
Joined: 3/11/2019 Last visit: 8/7/2024 Posts: 1545 Rating: (277) |
Hi, as a short test you can check the behaviour after deactivation of the itegrity check, like described here: After installing STEP 7 V5.7, why do you get a message about missing options packages when starting STEP 7?But nevertheless, you should check if the latest versions are installed (as well as for STEP 7 itself, means latest service packs and hotfixes, as well as for option packages). regards sancruz |
Feedback appreciated, please rate |
|
Follow us on