5/2/2017 5:31 PM | |
Joined: 9/27/2006 Last visit: 6/2/2024 Posts: 12259 Rating: (2670)
|
Hello garud; Have a look at the steps shown in the following FAQ: What are the options for connecting a PG/PC online to the S7 controller via Ethernet? Hope this helps, |
5/3/2017 8:20 AM | |
Posts: 51 Rating: (0) |
Ok. i can upload program by filling IP address of CPU . and Why i open accessible node and nothing in there . But In the other computer , i can see IP address node in accessible node . i use same IP address , same connector and what different ? |
Follow us on