2/16/2016 5:05 PM | |
Posts: 6 Rating: (0) |
We have this solution to configure an stepper motor (motor paso a paso),
with the manual solution it works (mode jok), but using move absolute
or move relative it desn't work.
Here we attach the example program.
Attachmentmotion control_2 - 1.zip (316 Downloads) |
2/16/2016 7:26 PM | |
Posts: 5225 Rating: (1188)
|
The configuration does not look right. Pulsing at 8 pulses/s (40mm/s) can surely not be right. You need a higher pulse rate.. Further - re-evaluate how the motion is triggered. Triggering is done on positive edge. Absolute motion is also not possible if the axis is not homed. Please use the forum search bar. The special manual is recommended: Good luck. |
Last edited by: William_B at: 2/16/2016 7:50:21 PMadd links |
|
This contribution was helpful to1 thankful Users |
3/24/2018 10:30 AM | |
Posts: 2826 Rating: (685) |
Hello.
Sharing the program will have the biggest chance for someone to analyze what issue is. Now taking a wild guess: Did you use MC_POWER? BR Update 1: |
Last edited by: #dP at: 3/24/2018 10:33:24 AM |
|