6/18/2009 12:06 PM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306) |
Hello Maverick85, |
6/18/2009 12:12 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hi Mav, I found this FAQ: PROFIBUS DP Diagnostics Blocks FB125, FC125 for SIMATIC S7 And about continue to work if some of slaves has fault look at Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? Hope this will helps. Best regards Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/19/2009 1:06 AM | |
Posts: 5 Rating: (0) |
Thanks UMENCHO that's exactly what I was looking for. I should have mentioned that the comms is over PROFINet. Thanks for all your suggestions. |
Follow us on