8/23/2022 2:27 PM | |
Joined: 6/2/2021 Last visit: 2/17/2024 Posts: 5 Rating: (0) |
Hello! I've done the hardware configuration and when I go online all looks ok but the problem is I don't receive nothing form the servo. I've seen something that I have to use PNIO_Send and PNIO_Recv but when I do this I get the error "System error or bad parameter type.". Also I think this will not help me so much because I have a standard FB from Festo to communicate with the servo and as a input of the FB I am supposed to write the Input address from the I/O link master. Does anyone now what I can do to make it work? Or it is even possible what I'm trying to do? Thank you! AttachmentScreenshots.zip (170 Downloads) |
Last edited by: Jen_Moderator at: 08/24/2022 09:40:03All files added as zip file. |
|
Follow us on