7/7/2006 10:30 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, i think you have to do a complete other way! The best are, you usethe area pointer "screen number". With this area pointer you know in your PLC, which picture currently show! In the second word of the area pointerstand the number of the currently picture. So if you know that picture xy shows and Q 0.0 = 1, then you can start in the PLC a counter. That will be the best. With a scriptthis will not be a good solution. Under the following Link, you will find the communication manual. There are all area pointer described. => http://support.automation.siemens.com/WW/view/en/1145110 In the attachment i put a smal sample project. greeting, AttachmentPicture_Number.zip (585 Downloads) |
Follow us on