8/26/2009 9:39 AM | |
Joined: 5/28/2008 Last visit: 7/12/2024 Posts: 4511 Rating:
|
Hello Jasner, If you are looking for ET200M fail safe modules for DO, here's bellow its data: 6ES7326-2BF01-0AB0 SIMATIC S7, DIGITAL OUTPUT SM 326, 10 DO; 24V DC, 2A, FAILSAFE DIGITAL OUTPUT FOR SIMATIC S7F SYSTEMS WITH DIAGNOST. INTERRUPT, 1 X 40 PIN 6ES7326-2BF40-0AB0 SIMATIC S7, DIGITAL OUTPUT SM 326, DO 8 X DC 24V/2A PM FAILSAFE DIGITAL OUTPUT P-M SWITCHING UP TO CATEGORY 4 (EN954-1), SIL 3 (IEC 61508) |
Ayman Elotaify |
|
8/26/2009 9:33 PM | |
Joined: 6/10/2008 Last visit: 6/29/2024 Posts: 186 Rating:
|
Hello miami, what do you mean by "morepossibilities with ET 200S"? Does ET200S failsafe station provides more safety then ET200M? The real question is this: is there any difference in ET 200M station which is used with failsafe modules and ET 200M for normal modules? Our idea is pretty much straightforward. We'll use failsafe CPU with failsafe modules and with software package "Distributed safety" hired professional PLC programmer will implement existing relay logic. |
8/27/2009 10:20 AM | |
Joined: 8/31/2005 Last visit: 6/14/2024 Posts: 2198 Rating:
|
Hello Jasner, In the ET300M you have the posibility to use F-DI and F-DO Modules, or standard modules and a 3TK28 to save switch off (the power supply of the standard DIO modules). In ET200S you can do the same, or use a F_PM module instead on the 3TK28. In this case you willnot need a extra unit, just replace the PM module(s) with a F_PM module(s). Have a look into the manual: http://support.automation.siemens.com/WW/view/en/12490437 In ET200M there is no simular modules to the F-PMs in ET200S. |
Last edited by: miami at: 8/27/2009 10:20 AM |
|
Follow us on