1/10/2010 1:27 PM | |
Joined: 10/7/2005 Last visit: 7/14/2024 Posts: 3009 Rating: (1053)
|
Hello Prats I presume by "ET200S+CPU" you mean an IM151-7 or -8 CPU, is this correct? If soyou may be able to use a seperate DP Master interface module for it (part number 6ES7 138-4HA00--AB0) which is available for later versions of the IM151 CPU's. I suggest you check thepart number of your CPU and see if you can find the DP Master interface for your ET200S CPU init's Step7 HWconfig catalogue folder (only really "old" IM151-7 CPU's do NOT support usage of this DP Master module). For completeness (and other usecases),Siemens do have a "Profibus to Ethernet" converter, it is called a "IE/PB link" and its part number is 6GK1 411-5AB00 (its main purpose is to be able to retain Profibus DP Slaves and link them to a Profinet I/O Master CPU). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
1/13/2010 7:09 AM | |
Posts: 272 Rating: (4) |
Thanks Fritz |
Follow us on