2/17/2010 8:51 PM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating:
|
Hello Gengus, Double check your wiring. Check the voltage delivered to Power Module. Do you have this 7VDC coming from the 8 outputs or only 2 of the 8? If it's a common problem in the 8 outputs then it's probably a problem with your 24VDC supply circuit. Make sure that load circuits are closed with 0VDC. If this problem happens to 2 outputs only then it's a mistake in theseoutputs' connection. Best regards. H-H |
Follow us on