7/22/2010 6:32 AM | |
Posts: 8 Rating:
|
Can we connect DP/DP coupler with S7 300R (cpu 315 2DP). As the DCS is on Profibus. |
7/22/2010 6:45 AM | |
Joined: 5/6/2010 Last visit: 3/13/2023 Posts: 11 Rating:
|
300 R system will communicate with dcs system over profibus via DP DP coupler http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=1179382&caller=viewmanual of DP DP coupler http://support.automation.siemens.com/WW/view/en/19281019check this link |
7/22/2010 10:57 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating:
|
Hello avi6630 ,
Although the software redundancy (SWR) solution is based on the ET200M (IM153-2), I believe you can still use DP/DP couplers. The point is that you will need 2 DP/DP couplers (One for eachDP master). In DCS, you will configure them as any 2 DP slaves on the same network. You should always inform the DCS which CPU is master or in other words which DP/DP coupler has the correct (latest) data because the DP/DP coupler of thestandby CPU will always have old deceiving data. Justpay attention to the followingparameters of FC 100 ‘SWR_START’. PAA_FIRST --- Number of first output byte used by an ET 200M with redundant-backup IM 153. PAA_LAST ---- Number of last output byte used by an ET 200M with redundant-backup IM 153. Output bytes in the range PAA_FIRST to PAA_LAST must form a contiguous range and may only be used by the ET 200Ms with redundant-backup IM 153s. SLAVE_NO ---- Lowest PROFIBUS address used for an ET 200M DP slave with redundant-backup IM153. SLAVE_LEN--- Total number of ET 200M DP slaves used.PROFIBUS addresses must be allocated contiguously. Do not count DP/DP couplers in these parameters. Best regards. H-H |
This contribution was helpful to
1 thankful Users |
7/23/2010 3:43 PM | |
Posts: 8 Rating:
|
Thank a lot. |
Follow us on