10/29/2010 6:27 PM | |
Posts: 1 Rating: (0) |
Hello! I'm trying to connect CPU 314C-2DP as Profibus DP slave to the S7-400H station via y-link. I have made the same steps as described in "Configuring an S7 CPU as DP slave on the H system using a Y-Link" example. But when I configure slave CPU 314C-2DP, the SF led is active, while BF led is ok. Diagnostic buffer of the cpu says that the slave isn't properly configured. Another slave device (Micromaster) in the same configuration operates well. I have double check the steps described and compare them with my project. And I have no ideas what the problem could be. I've attached the step7 project below. Any help will be really appreciated! Thank you! Attachmentylink_ex.zip (162 Downloads) |
Follow us on