7/22/2011 6:40 AM | |
Joined: 8/25/2006 Last visit: 8/13/2024 Posts: 2208 Rating:
|
Hello. Look at the manual, chapter 6.2. Look for diagnostics for DPV0. |
7/22/2011 9:13 AM | |
Posts: 25 Rating:
|
Hello KSN, Do you mean that the Diagnostics listed in the online-information is related to the Status byte 1-3? And so: LSB: 0 1: The DP master failed to address the DP/DP Coupler. • Have you set the correct PROFIBUSaddress on the DP/DP Coupler? • Is the bus connector connected? • Voltage on the DP/DP Coupler? 3MSB:5 1: The DP/DP Coupler has received a “SYNC” control command. |
Follow us on