10/7/2011 12:53 PM | |
Joined: 9/23/2005 Last visit: 10/17/2024 Posts: 4350 Rating: (1448)
|
Hi, That is the information that I get with the information stay on the S7-1200 manual, page "8.3.3 STATUS parameter for RDREC, WRREC, and RALRM": 0070-0100 00 = B#16#00, if no error 70 = 00 to 7F CPU No error or no warning 01 = 01 Reserved, reject Initial call; data record transfer has started C080-7F00 C0 = If no DPV1 protocol element is used, then B#16#C0 will be output. 80 = 80 DPV1 Error according to IEC 61158-6 7F = ?? I know that is not enough. I suggest you open a “Support Request” to get more information (maybe with developer). Tell us the information that you get... |
Last edited by: Pegaia at: 10/7/2011 12:54 PMDenilson Pegaia |
|
Follow us on