9/15/2005 1:21 PM | |
Posts: 3609 Rating:
|
Hi, I have ELS TP40M ind.eth. switch. since,it has MAC address on it, i assume, it is configurable? if so, what tools i need to configure it? br, marius |
9/15/2005 1:22 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating:
|
Hello Marius The “M” in the name of ELS TP40M means managed. Yes it is the one configurable ELS. The first step that you have to do is to give him an IP address (via DHCP, PST Tool, Step7). You find a good description about the configuration, diagnostics etc. in the manual under: http://support.automation.siemens.com/WW/view/en/13471140 PST download: http://support.automation.siemens.com/WW/view/en/19440762 Best regards Your Technical Support for Automation & Drives SIEMENS AG |
Follow us on