12/9/2011 10:58 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Yes, you need 24 VDC. There exist a diagnostic repeater. How do you determine the topology using the diagnostic repeater and display it in STEP 7 or read it out via the user program? Best regards, Hristo Mihalev |
12/9/2011 1:06 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread RS 485 Repeater. Best regards O_Moderator |
Follow us on