5/5/2007 5:11 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, That should work, did you check or the In- and Outputs are not mistyped somewhere in the program... For the Modbus communication you need the newest communication blocks, did you check that? This link doesn't seems to work... Is the 1SI Module up-to-date, see Operating system updates for ET200S 1SI (ASCII, Modbus)? See also the restrictions in the FAQ Which hardware components / interfaces can you use to connect the PtP CPs CP 340, CP 341 and the ET 200S 1SI module in a PROFIBUS DP, PROFINET IO network or to an IE/PB link? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on