10/27/2005 4:59 PM | |
Joined: 9/22/2005 Last visit: 11/5/2007 Posts: 7 Rating:
|
Hello saeed, for the standby-function you will need an ITP XP (Industrial Twisted Pair crossed) cable with 9 connectors to connect both OSMs. See http://support.automation.siemens.com/WW/view/en/8676999 regards marc |
10/28/2005 2:43 PM | |
Joined: 9/16/2005 Last visit: 2/6/2006 Posts: 39 Rating:
|
Hello saeed, hte standby mode is one the important functions within the redundancy function of the OSM. If you will configure a redundant ring one OSM must be in the Redunancy Master mode and other OSM are working as Standby Master or Standby Slave. For further information please refer the manual "Industrial Ethernet OSM/ESM Network Management" http://support.automation.siemens.com/WW/view/de/8677203/0/en Kind regards |
Follow us on