1/16/2008 8:39 AM | |
Posts: 30 Rating: (0) |
Hi. I have a CPU 224 and EM 277 with P-DP. I have to connect my WinCC 62 SCADA with comtroller through EM 277. Can I do it or it's impossible? Thanks. |
1/16/2008 9:51 AM | |
Joined: 9/27/2006 Last visit: 9/15/2024 Posts: 12282 Rating: (2683) |
Hello Serguey; Yes you can connect WinCC to a S7-22x using EM277 and a CP5613, as in the following FAQ: http://support.automation.siemens.com/WW/view/en/21915525 Hope this helps, Daniel Chartier |
1/16/2008 4:45 PM | |
Posts: 30 Rating: (0) |
Thanks for link...but Ihaven't CP 5613, I have 5611 on my PC...what about it?...or it only work with CP 5613? |
1/16/2008 5:14 PM | |
Joined: 9/27/2006 Last visit: 9/15/2024 Posts: 12282 Rating: (2683) |
Hello Serguey; The basic functionnalities with a CP5611 + Softnet drivers should be the same as a CP5613, especially if there is a small amount of data to be exchanged, The following FAQ mentions WinCC and S7-200 over CP5611:http://support.automation.siemens.com/WW/view/en/21915573Best thing I can suggest at this point is to try it out, we can look at any errors that occur. Worst comes to worst, You can use the CP5611 to connect to WinCC using MPI; other posts on the forum show it is easily done using the driver from MicroWin. |
1/17/2008 8:17 AM | |
Posts: 30 Rating: (0) |
There are SIMATIC NET cd in the software box....Must I install the Simatic Net....or the driver for CP 5611 is in the MicroWin? |
1/17/2008 1:41 PM | |
Posts: 1776 Rating: (95)
|
use the SIMATIC Net CD |
1/20/2008 3:35 PM | |
Posts: 5822 Rating: (412) |
Dear Sergey, you mentioned you have a DP 5412??? What Version of the SIMATIC NET CD do you have, on which OS of your PC? Best regards J_Bell |
1/23/2008 12:36 PM | |
Posts: 30 Rating: (0) |
SIMATIC NET 2006 whichwas contained in the box with WinCC 6.2 Windows XP SP2 |
Last edited by: Sergey_Lotvin at: 23.01.2008 12:40 |
|
Follow us on