7/27/2006 8:54 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
[quote user="Mrs NF"]How can send a data packet with lengh>240Byte? Hi, In the project you send me the triggering of the data is some odd, please look to the example program that is in the link. TheAG_SEND is only sending on a flank of the ACT-function!!! [:o] Sample program for the SEND-RECEIVE interface with the FC5 (AG_SEND) and FC6 (AG_RECV) blocks for S7-300 Whats on the Two PG/PC PC's? Some Application, normally that are "SIMATIC PC Station" with a IE General en een Application or/and a OPC Server.... I think you can't now send anything because thats working only once and there is no Application on the PG/PC... [:o] The question is, what do you want to make on the other side (on a PC) for application... |
Last edited by: Late at: 7/27/2006 9:00 PMPG/PC questions placed to it... I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on