7/28/2010 12:13 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
The IP data for the PROFINET interface is only retentive if the interface has been configured in HW Config and this configuration is also loaded on the IM 151-8 PN/DP CPU interface module, i.e. the SDBs must be available on the SIMATIC Micro Memory Card. Look at ![]() What about the program which you downloeded there? Do you use there any I/O? In the beginning you could download to the CPU some OBs - 80 to 89, also 121+122. Just to see what's happend there... Best regards, Hristo Mihalev |
7/28/2010 1:11 PM | |
Posts: 12 Rating:
|
HI I have tried to download a very simple code in OB1. And only download OB1. But it still makes the error. STL code in OB1: SET S M99.0 |
7/28/2010 2:08 PM | |
Posts: 12 Rating:
|
I’m missing the Busterminator, it’s on site in the electrical cabinet. Thanks, I’m not use to the IM151-8 CPU yet, normal I use 300 and 400 CPU’s. |
Follow us on