7/8/2019 3:55 PM | |
Joined: 8/14/2013 Last visit: 2/11/2021 Posts: 48 Rating: (1) |
Hello, first of all, thank you very much for so I am very confused and I do not know how . Thanks for the help you are giving me Attachmentmodbus6.pdf (106 Downloads) |
7/8/2019 4:23 PM | |
Posts: 3093 Rating: (323)
|
Hello, Regards, |
This contribution was helpful to1 thankful Users |
7/8/2019 4:37 PM | |
Joined: 8/14/2013 Last visit: 2/11/2021 Posts: 48 Rating: (1) |
It's false. That wants to say that itis not being executed, I suppose ... The block is called only once because it is in OB1 but it is called by bool "first scan". There is something more to tell you; when I "erase" or stop calling the modbus master module in OB1, the error in the CPU disappears ..... .Thank you Attachmentmodbus7.pdf (116 Downloads) |
Last edited by: cesarinko at: 07/08/2019 16:47:22 |
|
7/8/2019 5:51 PM | |
Posts: 3093 Rating: (323)
|
Sorry, I didn't insert the correct link. Second try: How do you evaluate the status of system blocks in STEP 7 (TIA Portal)? |
This contribution was helpful to1 thankful Users |
7/9/2019 6:25 PM | |
Joined: 8/14/2013 Last visit: 2/11/2021 Posts: 48 Rating: (1) |
Hello I have read several posts from people who have encountered this same problem. In my case, as in them, the parameters of parity, bit stop, speed ... etc are fine. I have also checked the connection cable and exchanged TX RX, I have checked the parameter Line_Pre ... etc I am learning to use the previous library (SaveStatus ") and I run into a problem. As I understand in the siemens support page, the link takes me to a website where the status status parameter is analyzed, like a 4-byte array. However the FB "SaveStatus", contained in the library that is downloaded from this page has an array of 10 DWord. I guess they are different things. I am analyzing the elements of the DB array corresponding to the "SaveStatus" of the master, but I do not know what part of the communication corresponds to each element of the array to be able to locate where the error is affecting. In the help of Tia Portal does not speak to me about this FB "SaveSTatus". Is there a page that explains what each element of the 10 in this array represents? Thank you Attachmentmodbus8.pdf (114 Downloads) |
Follow us on