8/31/2024 8:33 PM | |
Joined: 9/18/2022 Last visit: 9/6/2024 Posts: 1 Rating: (0) |
I know nothing of whether there is a magic way to make it auto-see the festo servo drive. However, I will say that any drive you can connect to the s7-1500, and make run, you can actually connect to the CNC. It will not auto-detect them but you can set them up manually. You also may have to simulate the telegrams depending on what you have. See https://support.industry.siemens.com/cs/ww/en/view/109823551 for an example of how to add an axis/motor that is just communicating through process image and IO without it being auto-detected. See https://support.industry.siemens.com/cs/ww/en/view/109821327 for a library that can simulate the basic telegrams for you. You can connect this all together to basically run any servo (or vfd) with a little work if it can be run already. I actually simulate an indexing axis this way for a toolchanger that uses a third party VFD, and really only understands CW/CCW commands (obviously i could rewrite the tool changing tot not use a real axis, but this was simple enough) |
Last edited by: DannyBee at: 08/31/2024 20:34:03Last edited by: Moderator_Lan at: 09/02/2024 09:31:21link optimized Last edited by: Moderator_Lan at: 09/02/2024 09:32:10 |
|
Follow us on