1/20/2018 9:07 AM | |
Posts: 6 Rating: (0) |
hallo please help me i have a problem with a control Sinumerik SBL 500 in a machine the alarm is : ( 25201 Axis z1 drive fault ) can somebody help me ? thank you . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/22/2018 10:40:30 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
1/22/2018 10:35 AM | |
Posts: 6 Rating: (0) |
Hallo Piscean 2010 the alarm is ( 300608 ) and this messages ( Axis x1 drive 1 speed control output limited ) how can i solve the problem and Thank you very much |
1/23/2018 5:10 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello mazentuma, Alarm 300608 = Speed controller at limit, means speed controller out put stays at its limit for too long time, check if the mchanical load is too high, motor is jam (Brake not released), etc. etc. PLease check if MD 1605, 1606 & 1105 & refer those with original data back up. HTH. |
This contribution was helpful to1 thankful Users |
1/24/2018 12:11 PM | |
Posts: 6 Rating: (0) |
Hallo piscean2010 please help me to access to the window values MD1605 & 1606 step by step ^_^ Thank you for your help. |
1/30/2018 5:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello mazentuma From your past posts, I assume that sombody has played with mechine data values. Whenever you try to solve one problem, lands into anoter one. So to solve this problem once for all, I suggest you to reload the machine back up. Please ensure you have good working machine back up. Or other wise trial & error methods like the present one, will cost you time & machine down time. HTH. |
Follow us on