1/26/2018 7:18 AM | |
Joined: 10/11/2006 Last visit: 5/30/2024 Posts: 5854 Rating: (793)
|
Hello Louis, all our winder applications (Simatic, Simotion and Sinamics DCC) have the V-constant control mode. It is exactly what you require. The web speed (from tachometer running on the material) and the winder shaft actual speed are used to calculate the diameter. The material web velocity setpoint is then divided by the diameter to calculate the required winder shaft speed. Attached the general description of this mode. Attachmentpages from 38043750_DCC_Winder_en_V4_2_2.pdf (879 Downloads) |
With best regards, |
|
Follow us on