8/8/2022 8:38 AM | |
Joined: 9/19/2018 Last visit: 12/6/2024 Posts: 399 Rating:
|
The description applies to all versions of LOGO!8 Pure (LOGO!8.1 or newer). There is no firmware update for older LOGO!s. Handling: - Switch on the LOGO! power supply during a Micro SD card with the firmware update is inserted. No other files should be on the card. - The LED on the front of the LOGO! Pure flashes as long as the firmware update is performed. - After the firmware update has been completed, the LED lights up constantly (the color depends on whether a user program is included). Hints: The current firmware update of a LOGO! 8.3 (to V1.83.02) is available at the following link: Update of LOGO! 8.2: Update of LOGO! 8.1: Since the software is export restricted, you may have to register beforehand. When registering, check on "Access authorization for downloading export restricted software", see: LOGO! Support |
This contribution was helpful to
1 thankful Users |
8/8/2022 4:49 PM | |
Joined: 12/18/2014 Last visit: 9/19/2025 Posts: 36017 Rating:
|
For the LOGO!s 8.1 and 8.2 there are newer firmware updates from July 7th, 2020, which fix security problems. Product information on the firmware update for LOGO! 8 for security Vulnerability CVE-2020-7593 |
Follow us on